This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: required hardware for gesture detection

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843ISK

Hello,

I'd like to set up an environment to detect and recognize hand gestures. 

There should be the possibility to not only use the existing gestures but define my own ones out of the radar signal patterns. 

Is it right that I'll need the the DATA-CAPTURE-BNDL additionally to the IWR1443BOOST or is there anything else required?

And do I need an additional LaunchPad development kit or is it enough to just connect the IWR1443BOOST to the PC and the LaunchPad kits are only optional?

Thank you very much in advance

Best wishes