Dear Engineers,
There are 2 problems about LMT70~
1 What are the requirements for the ADC accuracy and other parameters of the back end (customers consider using the ADC embedded in the MCU)? Is there a reference code suggestion?
2 If the LMT70 is used in a smart watch, after the calibration of the previous prototype stage, in the mass production process, does each watch still need a regional calibration temperature?
Looking forward to your reply!
Thanks
Robin