This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2080: HDC2080 - wrong humidity

Part Number: HDC2080


Hi All,

I get right temperature from HDC2080, but humidity is very low. From 15% to 26% for real humidity 67% (measured by psychrometer with two thermometers).

I wait several days after soldering - no change.

If I make 100% humidity near sensor (drop of water directly to sensor window) - I get 80%-90%.

And after I remove water from sensor during 10 minutes I get again 26%.

?