This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-C2000EVM: Setup for Fluid Concentration

Part Number: TDC1000-C2000EVM


Hi,

I am using the TDC1000-C2000EVM for fluid concentration. Currently setup is two transducers (Steminc SMD07T05R412WL, 4.25MHz) mounted, transducer 1 connected to TX1 and GND and transducer two connected to RX1 and GND. The transducers are mounted to a plastic wall, with the transducers being approximately 20mm apart from each other. Configuration is set to mode 1 with channel 1.

The problem is that the measurements do not make sense. When the tank is empty (no water) the measurement is still the same. Even when transducer 2 (RX1) is disconnected, the measurements do not change.

Can you please assist in finding the error and give recommendations to setup parameters?

Regards

Jon Anders Øgaard