This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112: Getting temp reading above 128C in 12-bit configuration

Part Number: TMP112
Other Parts Discussed in Thread: TMP117

Hello!

I need to use TMP112A sensor to measure temperatures upto 160C. The datasheet mentions that the sensor should be configured in 13-bit mode to read temperatures above 128C. I want to be able to read 160C temperatures in 12-bit mode itself (some communication format related constraint at my end). Is that possible? More specifically, what would the sensor output be (in 12-bit configuration) for 135C temperature (say)? Would it be 1000 0111 0000 or will there be no output at all?

Thanks,

Swantika