Other Parts Discussed in Thread: IWR1642
Setup - Windows 10, IWR1642BOOST, Chrome Ti Cloud agent Bridge extension installed.
I installed mmwave SDK in C:\ti - this was the default suggested by installer
installed CCS 8 in C:\ti
IWR1642 boost board connected and com ports are appearing on the computer.
When I visit the mmwave visualizer website it asks me to install the ticloudagent_2.exe
When I run this executable, it comes with a default installation location C:\username - when I try to install it in a directory C:\username\cloudagent - it goes on to extract, a popup comes stating settingup system which will take some time at this point a windows error dialog pops up with a red X stating "appdata\local\texas not found"
What is it looking for and where should I be installing it so that it can find what it is looking for.