Thanks for your supports,
>test 1, the IWR6843ISK is assembled above 1.2 meter from gound; the ange is 0 degreen between wall and IWR6843ISK baord;
downlaod the lab21 profile "area_scanner_68xx_lab.bin", in the file "mmw_area_scanner_68xx.cfg" , off the clutterRemoval, "clutterRemoval -1 0" , then tes the object; if the objects is moving, the detection distance is more than 10 meter; but if the objects is statics, the maximal detection distance is about 2 meter; Could you please help us how to increase the dectection distance for static objects?
>test 2, the IWR6843ISK is assembled above 1.2 meter from gound; the ange is 0 degreen between wall and IWR6843ISK baord;
>downlaod the lab0017_mmwave_sdk_68xx profile "xwr68xx_mmw_demo.bin", then tes the object; if the objects is moving, the detection distance is more than 10 meter; but if the objects is statics, the maximal detection distance is about 2 meter; Could you please help us how to increase the dectection distance for static objects?
>test 3, the IWR6843ISK is assembled above 1.2 meter from gound; the ange is up 10 degreen between wall and IWR6843ISK baord;
downlaod the lab21 profile "area_scanner_68xx_lab.bin", in the file "mmw_area_scanner_68xx.cfg" , off the clutterRemoval, "clutterRemoval -1 0" , then tes the object; if the objects is moving, the detection distance is more than 10 meter; but if the objects is statics, the maximal detection distance is about 2 meter; Could you please help us how to increase the dectection distance for static objects?
>test 4, the IWR6843ISK is assembled above 1.2 meter from gound; the ange is up 10 degreen between wall and IWR6843ISK baord;
>downlaod the lab0017_mmwave_sdk_68xx profile "xwr68xx_mmw_demo.bin", then tes the object; if the objects is moving, the detection distance is more than 10 meter; but if the objects is statics, the maximal detection distance is about 2 meter; Could you please help us how to increase the dectection distance for static objects?