This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: AWR1642 TX power reduce setting through configure file?

Part Number: AWR1642


Sir,

Can I setup the TX output power reduce 6dB through the profileCfg of configure file from  

profileCfg 0 79.0 5 5.7 28.87 0 0 64.9 1 128 5769 0 0 34

into

profileCfg 0 79.0 5 5.7 28.87 6 0 64.9 1 128 5769 0 0 34

?

If yes, is this setup related to both of TX of AWR1642 at the same time? If yes, can I setup different reduce value for both TX through profileCfg? Can you show the example for my reference?

JY