This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: The detection object of doppler is affected, after turn off clutterRemoval

Part Number: IWR6843ISK

Thanks for your supports.
>Question 1,

IWR6843ISK is assemble on the wall about 1.2 meter above ground, the board Z+ is forward ground, the angle is 0 between the board and wall;

run the lab0021_area_scanner_68xx;
the profile is attached, based on default mmw_area_scanner_68xx.cfg, have changed the below: clutterRemoval -1 0; cfarCfg -1 0 0 8 4 4 0 256 0; aoaFovCfg -1 -45 0 -90 90; cfarFovCfg -1 0 0.4 8;
the test resault is below:

normally, place a metallic object which size is 70cm(height) X 40cm(width), the distance is 3.3meter; in log_data.csv of lab21,
mostly, location of the object is right; but sometimes the loaction of the object is wrong which Z is mirror; the Z should be 0.5meter, but sometimes the Z is -0.5meter;
could you please help us?


>Question 2,

IWR6843ISK is assemble on the wall about 1.2 meter above ground, the board Z+ is forward ground, the angle is 0 between the board and wall;

run the lab0021_area_scanner_68xx;
the profile is attached, based on default mmw_area_scanner_68xx.cfg, have changed the below: clutterRemoval -1 0; cfarCfg -1 0 0 8 4 4 0 256 0; aoaFovCfg -1 -45 0 -90 90; cfarFovCfg -1 0 0.4 8;
the test resault is below:

normally, there is no moving object before IWR6843ISK ; in log_data.csv of lab21,
mostly, there is no the object of doppler; but sometimes, there is a object of doppler in on frame, according to the location in log_data.csv, but there is no any static object and there is no any moving object.
could you please help us?