This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Cannot install XDS110 driver in Win7

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443, CC1350

Hi,

I'm having trouble installing drivers of XDS110 devices in Win7, like IWR1443 evm board, c6678 DSP, CC1350 MCU etc.

The device manager display all these device as "XDS110 (02.03.00.11) Embed with CMSIS-DAP". Windows cannot find a driver if I try to update the driver, or uninstall the device and replug it. But all the devices can be recognised on other machines if CCS is installed. 

I've also tried changing the cable, changing the USB port, rebooting computer, reinstalling CCS and EMUPack but none of them worked. 

May I have some help with this?

Thanks,

Han