This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP1075: Conversion current included in quiescent current ?

Part Number: TMP1075

Hello,

I see in the datasheet a Quiescent current at 2.7µA (typical) at conversion rate = 220ms.

There is also a 52µA (typical) conversion current.

My question : is the conversion current (52µA during 5.5ms every 220ms) included in the 2.7µA quiescent current or do I need to add it ?

In other worlds, can I considere that 2.7µA is the overall average current when configuring the sampling rate at 220ms with no I2C reading ?

Regards,

Thierry