This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP102: Is the connection of the address pin latched at power on?

Part Number: TMP102
Other Parts Discussed in Thread: TMP112

Team,

A question has come up as to the operation of the TMP102 and TMP112 sensors. 

Is the connection of the address pin latched at power on (ie fixed address for duration of power-on), or is the address of the device dynamic if the address pin is driven to different locations during operation?

Why does this matter?  Our FMEA analysis revealed that undesirable behavior might happen if the A pin were floating or coupled loosely to other signals.  I argued that it ought to be latching the address at power on, but I can’t seem to find any evidence of that in the datasheet.

Thanks

Viktorija