Part Number: TDC1000
Other Parts Discussed in Thread: TDC1011
Hi,
Trying to develop a sensor system with TDC1000 / TDC1011 for concentration reading of a specific liquid in a temperature range 10-40C. Build a measurement chamber from plastic , using x1 transducer of 1Mhz, and a microcontroller to read TOF values from the TDC. At constant room temperature everthing seems to be ok, there is strong echo returning and the START-STOP signals are also readible. Tried almost all settings of the TDC and also putting the sensor to outside of the wall of the chamber OR drilling a hole and putting the sensor surface directly relation with the liquid.
The problem is ; when you change the temperature high or low, the shape of the echo changes slightly, like amplitude of the first pulse changes or the order of positive and negative pulses change. And this affects the treshold trigger of the system which in relation affects the tof results. As an example lets say you have 5 pulse echo ( 5 up and down cycles ) , at 20C because of the amplitude of the first pulse the STOP is triggered with the first pulse but at 40C the amplitude of the first pulse decreases ( but still strong enough) and as it is under the level of treshold, the next pulse which has a bigger amplitude causes the trigger, in the end the result changes at least 1 pulse width.
Tried to average various number of readings, or some error catching algorithms but withoud any good results, since the change of the trigger is huge!
Do you experience such a thing, can you think of any solution or idea about the problem ?