This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Pre-program or Flash AWR1243 to run in a specific configuration

Part Number: AWR1243

Hi,

I want to pre-program AWR1243 to run in a specific chirp configuration on every re-start.

I understand that the normal process is to use a host processor to program the default binaries and then send SPI commands to set the configuration. This is usually done with Processor SDK (Radar) in TDA3x.

I do not want to use any host processor and I want to freeze a configuration and on every restart, I want the AWR1243 to start transmitting the programmed/flashed config.

Is this possible? if yes, please help me on the steps.