Other Parts Discussed in Thread: MMWAVEICBOOST,
Hi:
Our team has tested the IWR6843ISK+MMWAVEICBOOST unit for a while.
We have some more questions, as below:
- For sweep bandwidth of 500MHz (between 61.0 and 61.5GHz), what is the measured power (or Effective Radiated Power ) and its variation across the 500 MHz segment?
- For sweep bandwidth up to 4.0GHz (60.0 – 64.0GHz), what is the measured power (or Effective Radiated Power ) and its variation across the 4 GHz segment?
- If possible, could you show the Spectrum Analyzer screen shots of 1 and 2 above?
- Is an additional (10 to 15 dB or so) Rx preamp possible to be added to IWR6843ISK? If possible, how?
Thanks.
Ziyou