This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000: LMP91000 bias in StandBy mode

Part Number: LMP91000

In the standby mode, the TIA is OFF, while the A1 control amplifier is ON. This mode of operation is suggested when the gas detector is not used for short amount of time and a faster warm-up of the gas detector is required.

According to the data, shorting CE and RE can measure the bias voltage, but the bias voltage disappears after entering the StandBy mode after setting the bias voltage.

register

address value
0x00 0x00
0x01 0x00
0x10 0x05
0x11 0xdd
0x12 0x82