This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM26: Operating at -62C Temperature

Part Number: LM26

Hi Team,

My customer wants to be able to store their system for up to 365 days at -62°C. They wish to apply power without damage (not operate until the temperature reaches -40°C). They would like to implement this protection using the LM26CIM5-BPB. However, its operating temp is -55C (-65C storage). Would it be possible for them to apply power at -62°C without damage?

I assume they can't do that since it violates the spec but just want to confirm.

Thanks,

Antonio

  • Hi Antonio,

    As you know, LM26 has an Absolute Max Storage Temperature of -65C and a Recommended Operating Temperature of -55C. If the device is powered on below -55C, we don't expect the device to be damaged. However, the device may not operate as expected and the output may be incorrect. We don't guarantee operation below -55C.

    Thanks,
    Ren