Hi,I use the recommended setting,but when i push the SEND CONFIG TO MMWAVE DEVICE button,There is an Error in the last of the Console Messages,It means that the sensor can't run. Please give me some advises.Thanks very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,I use the recommended setting,but when i push the SEND CONFIG TO MMWAVE DEVICE button,There is an Error in the last of the Console Messages,It means that the sensor can't run. Please give me some advises.Thanks very much.
I have met the same error before. It works only when you flash demo from SDKV1.2.
Because the chip in your board is vision ES1.0, you can check it with the number '502' in your chip.
This chip is early chip version,and it can only use SDKV1.2 and the vision previous.