This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: Failing to flash

Part Number: IWR6843ISK-ODS
Other Parts Discussed in Thread: UNIFLASH, , IWR6843ISK, MMWAVEICBOOST

Hello

I have an IWR6843ISK-ODS which is failing to flash an image using UniFlash.

It hangs on Load Program (Opening COM port COM4).

I also have an IWR6843ISK which I can flash multiple different images successfully.

In both cases (IWR6843ISK, IWR6843ISK-ODS) I use exactly the same other software and hardware including

  • MMWAVEICBOOST
  • Windows laptop
  • Power supply
  • USB cable
  • Uniflash

Is there anything I can do to debug this or do I simply have a dud board for the IWR6843ISK-ODS?

Best Regards

David