Hi,
I am also having problem with the depthCamera->registerCallback(Voxel::DepthCamera::FRAME_RAW_FRAME_UNPROCESSED, (DepthCamera::CallbackType)frameCallback);.
I get an access violation.
My Callback Foo is defined as "static void frameCallback(DepthCamera &dc, const Frame &frame, DepthCamera::FrameType c)".
My environment is MS2017 and I am using the lib and dll 's as installed with voxel-0.6.10.
The app I am making is strictly a Win32 app. It is basically a stream to file program that uses the UNPROCESSED data.
I can find the camera and read and write the registers but I can't set a call back.
Any help would be appreciated.
Thanks,
K