Other Parts Discussed in Thread: IWR1642
Hi,
I'm using the IWR1642BOOST board with a DCA1000 to capture raw packets.
I'm also using the default SDK firmware in the IWR1642.
I'm wondering how I can compute the number of chirps per frame, because the amount of captured data with the DCA1000 does not match my expectations ?
So something is wrong in my computation !
Parameters, according to profile (see below):
- 4 RX channels, complex I/Q -> 8 samples
- 256 samples per chirp (sampling frequency is 5500 KHz)
- 2 chirps profile '0' and '1' + 32 loops ==> should be 64 chirps per frame ???
So, for one frame of 100 ms, I should receive 8x256x64 samples. Samples are 16-bit. So total amount of raw data should be 262144 bytes (256 KB),
but I receive twice this amount of data (512 KB per frame).
So what is wrong ?
Thanks
OG
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 77 7 7 58 0 0 68 1 256 5500 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 32 0 100 1 0
bpmCfg -1 0 0 1