This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000: SNAA287A 400KHZ VALUES

Part Number: TDC1000
Other Parts Discussed in Thread: LMV881, OPA357,

Hello,

I'm trying to replicate Åckerberg-Mossberg Filter using OPA357. With the SNAA287A as reference, how can I get 400kHz center frequency?

The selected values are:

R4=R5=R3=R6=4.3K

C2=C3=91pF

C1=1nF

R1=6.8K

R2=66K

Rout1=1.5K

Rout2=8.2K

Cout1=2.7nF

Rc=2K

I'm not sure I got all values right. Any comments/suggestions?

Thanks!