Other Parts Discussed in Thread: PGA450Q1EVM, , TIDA-00151, PGA460-Q1
I am using the PGA450-Q1EVM-S at a supply voltage of 8V. I am not using PGA450Q1EVM board for evaluation. I am connecting external microcontroller to configure the module.
I would like to use SPI interface to communicate for the distance measuring. But I do not know how to use SPI to read the receive signal for the distance measuring.
I came to know that the micro is to be in the RESET state, then the EN_CTRL's BURST_A_EN bit must be toggled from 0 --> 1. After this the FIFO start to fill.
What are the commands to excite the transducer (EN_CTRL's BURST_A_EN) and to configure the ultrasonic transmission by using SPI?
What are the commands for short distance and long distance measurement by using SPI communication?
To calculate distance, What are the blanking time and downsample values for PGA450-Q1EVM-S as it is already programmed?