Other Parts Discussed in Thread: AWR1443
Hi,
Im having problems running the mmwave sdk demo with demo visualizer on my awr1443boost es2.0 kit. I am running ccs 8.3.
I imported the project from resource explorer industrial toolbox v2.3.1 (based on this dev.ti.com/.../labs.html)
I import the "mmwave SDK Demo - 14xx" from the industrial toolbox.
I rebuild it as is (using mmwave SDK 1.2.0.05)
I then launch the code on the mmwave chipset and connect it to the demo visualiser 3.1. When i try to configure it I get now the following:
mmwDemo:/>% ***************************************************************
Skipped
mmwDemo:/>% Created for SDK ver:01.02
Skipped
mmwDemo:/>% Created using Visualizer ver:3.1.0.1
Skipped
mmwDemo:/>% Frequency:77
Skipped
mmwDemo:/>% Platform:xWR14xx
Skipped
mmwDemo:/>% Scene Classifier:best_range_res
Skipped
mmwDemo:/>% Azimuth Resolution(deg):15
Skipped
mmwDemo:/>% Range Resolution(m):0.044
Skipped
mmwDemo:/>% Maximum unambiguous Range(m):9.01
Skipped
mmwDemo:/>% Maximum Radial Velocity(m/s):1
Skipped
mmwDemo:/>% Radial velocity resolution(m/s):0.13
Skipped
mmwDemo:/>% Frame Duration(msec):100
Skipped
mmwDemo:/>% Range Detection Threshold (dB):15
Skipped
mmwDemo:/>% Range Peak Grouping:enabled
Skipped
mmwDemo:/>% Doppler Peak Grouping:enabled
Skipped
mmwDemo:/>% Static clutter removal:disabled
Skipped
mmwDemo:/>% ***************************************************************
Skipped
mmwDemo:/>sensorStop
Done
mmwDemo:/>flushCfg
Done
mmwDemo:/>dfeDataOutputMode 1
Done
mmwDemo:/>channelCfg 15 5 0
Done
mmwDemo:/>adcCfg 2 1
Done
mmwDemo:/>adcbufCfg 0 1 0 1
Done
mmwDemo:/>profileCfg 0 77 429 7 57.14 0 0 70 1 240 4884 0 0 30
Done
mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1
Done
mmwDemo:/>chirpCfg 1 1 0 0 0 0 0 4
Done
mmwDemo:/>frameCfg 0 1 16 0 100 1 0
Done
mmwDemo:/>lowPower 0 0
Done
mmwDemo:/>guiMonitor 1 1 0 0 0 1
Done
mmwDemo:/>cfarCfg 0 2 8 4 3 0 1280
Done
mmwDemo:/>peakGrouping 1 1 1 1 229
Done
mmwDemo:/>multiObjBeamForming 1 0.5
Done
mmwDemo:/>clutterRemoval 0
Done
mmwDemo:/>calibDcRangeSig 0 -5 8 256
Done
mmwDemo:/>compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
Done
mmwDemo:/>measureRangeBiasAndRxChanPhase 0 1.5 0.2
Done
mmwDemo:/>CQRxSatMonitor 0 3 5 123 0
Done
mmwDemo:/>CQSigImgMonitor 0 119 4
Done
mmwDemo:/>analogMonitor 1 1
Done
mmwDemo:/>sensorStart
Debug: Init Calibration Status = 0x7fe
Exception: ../main.c, line 1748.