Tool/software: Linux
Hello, Guys:
Now I am working on IWR1642 platform for a radar module, The first version of the demo can working now, But it just very simple function version.
I have below issues need to fix:
1) Are there any way to set the IWR1642 in low power mode which core current is less than 5mA ??
2) How can I set IWR1642 make system level self checking and what is the software interface in SDK??
3) Base on current IWR1642 hardware platform can we find a way to make our source code safety, It means our source code and our application can not be hacked easily??
wait for your suggestion :)
RZ