Other Parts Discussed in Thread: UNIFLASH, , AWR1642BOOST, AWR1642
I cannot program the board. Out of box, the board worked fairly unreliably with the Visualiser tools with multiple power cycles required to get the software to recognize and run the demos. I attempted to change the firmware so that I could use the high precision range demo. since then , it has not functioned. I have used the Uniflash programmer both on -line and local and it informs me that the XDS 110 firmware is out of date. I have successfully updated this firmware using Uniflash. I am trying to reprogram the board with the following xwr16xx_radarss_rprc.bin from the mmwave_sdk_03_01_01_02 directory. Before I return the board (I assume that it is damaged )- do I have the correct firmware / configuration ? ( BTW I have the 101 jumper configuration) The chip has Uniflash is never able to identify the processor the 502AC marking automatically.
the following messages are fairly typical -