Hi,
I am working on a project, where I have to detect animals or human from high magnetic field area. I need a sensing system with a maximum 20 cm detection range. I already tried FDC10044evm but somehow it works not so good in a magnetic field. It seems too much fluctuation in the results (without object). And with the object within the range of 5 to 10 cm, the sensor was detected nothing.
In that situation, TI can suggest a solution or is there any other Capacitive proximity sensor?
Thanks