This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: 3.3 V and 5V connectors

Part Number: AWR1642BOOST

I want to use the 3.3V and 5V (1 and 2 on J6) connectors in order to power an external microcontroller but when I probe them they both are 0V. Is there a pad somewhere on the board that needs a 0 ohm resistor? And yes I am getting power to the board because I measured 5V on P5.