This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/IWR1443BOOST: Problems Flashing IWR1443Boost

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH, IWR1443

Tool/software: TI-RTOS

Hello,

I want to Flash the IWR1443Boost, that i can debug with the CCS. The Board is ES3. I have tried to Flash with the SDK 2 and 3 but there is always the following error in uniflash:

[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Initialization complete.
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Flashing process starting...
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Connecting to COM Port COM5...
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Reset connection to device
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Set break signal
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Reading device version info...
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: ** 2 files specified for flashing.
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Checking file C:/ti/mmwave_sdk_03_01_01_02/firmware/radarss/xwr12xx_xwr14xx_radarss_rprc.bin for correct header for IWR1443.
[9.4.2019 12:44:21] [INFO] Cortex_R4_0: Header of C:/ti/mmwave_sdk_03_01_01_02/firmware/radarss/xwr12xx_xwr14xx_radarss_rprc.bin file indicates it is not a valid file to flash to IWR1443: 0x43525052
[9.4.2019 12:44:21] [ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!
How can I solve this?
Thank you
Raphael