Other Parts Discussed in Thread: UNIFLASH
Tool/software: Linux
Hello,
Unfortunately, I need to run my application on Linux and I have a couple of set-up problems.
On windows everything was working properly so, it is definitely something that I am doing wrong in my setup.
I have my own version of the object detection but I still need to input the COM ports to make it run. I thought it is because I did not reflash the radar, so I also tried doing the entire procedure of flashing using uniflash, but I still need the ports #. I tried with /dev/ttyACM0 & /dev/ttyACM1 and it does something compared to others where it just sends an error instantly, here it outputs error: Not able to connect to serial port. Recheck the COM port selected.