This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Minimum Distance for Object Detection

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Is there a minimum distance the IWR1443 has at which it can detect objects? Attached the config file being used for your reference.

Also, can I know if there is a formula to calculate it, and what parameters in the sensing estimator affect it?

Thanks.1443_3d_profile.cfg