Other Parts Discussed in Thread: AWR1642BOOST
Hi,
I'm looking at the Short Range Radar Reference Design TIDEP-0092 Resets and LEDS schematic and I'm struggling to understand how R103 can be 510 Ohms given that Q1 N-channel Mosfet (BSS123) has a drain current (Id) of 0.17A and Rds(on) @ 4.5V is 10 ohms. So Vds = 0.17A x 10 Ohm = 1.7V.
The LED at the drain of Q1 is TLMY1000-GS08 whose forward voltage (Vf) is 1.8V. So by my calculation, R103 = (5V - Vds - LED's Vf) / Id = (5V - 1.7V - 1.8V) / 0.17A = 8.82 Ohms, but R103 is 510 ohms per TIDEP0092. I'm propably missing something.
Thanks,
John