This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: Momoshot and continuous mode

Part Number: OPT3101

Hi team,

There are continues mode and monoshot mode.

We need to make sure that capture is accurate and simultaneous with our motor.

The process is: sync --> continue capture n data--> sync, n will depends on motor speed.

We have few questions in below.

1. In monoshot mode, we do trigger, can that shot to shot in 555uS(1.8KHz)?

POWERUP_DELAY= (64 × POWERUP_DELAY + 2) × tCLK,and power delay can be in 50nS?

2. In continues mode, can we change sample rate and then trigger first frame start?

And how long can generate first frame after change sample rate?

Thank you!

Hi team,
There are continues mode and monoshot mode.We need to make sure that capture is accurate and simultaneous with our motor.The process is: sync --> continue capture n data--> sync, n will depends on motor speed.We have few questions in below.1. In monoshot mode, we do trigger, can that shot to shot in 555uS(1.8KHz)?POWERUP_DELAY= (64 × POWERUP_DELAY + 2) × tCLK,and power delay can be in 50nS?Hi team,
There are continues mode and monoshot mode.We need to make sure that capture is accurate and simultaneous with our motor.The process is: sync --> continue capture n data--> sync, n will depends on motor speed.We have few questions in below.1. In monoshot mode, we do trigger, can that shot to shot in 555uS(1.8KHz)?POWERUP_DELAY= (64 × POWERUP_DELAY + 2) × tCLK,and power delay can be in 50nS?
2. In continues mode, can we change sample rate and then trigger first frame start?And how long can generate first frame after change sample rate?Thank you!