This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: IWR1143 Wireless communication

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: TIDEP-0091

Hello,

I bought an IWR1443BOOST board and I would like to make a tank level application for measuring solids. I would like to send level information wirelessly (Using CC1312 for example) and be able to change parameters from a pc/web/phone application. My questions are the following:

1. Is it possible to process the data directly from IWR1443BOOST firmware to get the real level and send it to the wireless module throught SPI/UART/I2C

2. Is there any example I could use to start my project?

Thank you in advance,

Jorge