Other Parts Discussed in Thread: OPT9221
After powering up OPT8241-CDK-EVM I need to turn the sensor on and off several times to get a noise-free point-cloud and images. What could be the problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
After powering up OPT8241-CDK-EVM I need to turn the sensor on and off several times to get a noise-free point-cloud and images. What could be the problem?
Hi,
I am running from Voxel Viewer. However, I think it was the USB port I was using - I changed ports on my machine and haven't experienced the problem since. I do have another question though - when I use VoxelSDK to extract the depth and amplitude maps I don't have any issues, however when I change the sensor parameters and try to extract the raw data (DepthCamera::FRAME_RAW_FRAME_UNPROCESSED), it causes the Voxel Viewer to freeze and I get the following contents in the log:
ERROR: USBSystem: Could not get node name of device = 9 connected to USB hub device = '\\.\USB#ROOT_HUB30#4&186df573&0&0#{f18a0e88-c30c-11d0-8815-00a0c906bed8}'
INFO: ParameterDMLParser: Found register map with name 'OPT9221' (vPG1P0)
INFO: HardwareSerializer: Received 42909 bytes from hardware in 1.93083 s
INFO: Data2DCodec: Original number of 8-bit offsets = 256
INFO: Data2DCodec: Number of invalid pixels in original data = 0
INFO: Data2DCodec: Current number of 8-bit offsets = 256
INFO: CameraSystem: Successfully refreshed parameters for TintinCDKCamera(0::0451:9105::12019311199913).
INFO: ToFCameraBase: Starting with 320x240@30.0001fps
WARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline.
WARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline.
WARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline.Using rate factor = 0.1
Using rate factor = 0.308758824615
Using rate factor = 0.13579507422
Using rate factor = 0.11436934291
C:\PROGRA~1\TEXASI~1\VOXELV~1.10\VOXELV~1\pyqtgraph\graphicsItems\ImageItem.py:354: VisibleDeprecationWarning: using a non-integer number instead of an integer will result in an error in the future
WARNINGWARNINGWARNINGWARNINGWARNING: USBBulkStreamer: Dropping a frame because of slow forward pipeline.
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '307200' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530530411904
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '0' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530530825797
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '307200' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530531144942
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '0' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530531558835
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '307200' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530531877981
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '0' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530532291874
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '307200' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530532612018
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '0' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530533025910
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '307200' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530533345058
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '0' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530533758949
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '307200' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530534011275
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '0' bytes
WARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530534425166
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERRORWARNING: USBBulkStreamer: Resetting bulk endpoint at 1555530534745311
ERROR: USBIO: Could not transfer '307200' bytes
ERROR: USBIO: Could not transfer '0' bytes
ERROR: USBIO: Could not transfer '0' bytes
WARNING: