Is there a minimum or maximum inductance the LDC1101 can measure?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks, my coil can measure between 2 positions (extended and retracted) (I have a sliding magnet inside my coil)
I used the network analyzer method and measured at both 500KHz and 10MHz, and then measured at the resonance frequency.
Retracted measurements:
F=500kHz Rs=254 Xl=1510 Rp=8970
F=10MHz Rs=64 Xl = -395 Rp=2430
Fresonance=1.21MHz Rs=17.3K Rs=-5.48K Rp=1735
Extended measurements:
F=500kHz Rs=214 Xl=1860 Rp=16166
F=10MHz Rs=65.9 Xl = -417 Rp=2638
Fresonance=1.12MHz Rs=23.5K Rs=-3.66K Rp=570
Based on these measurements, what would you recommend for Cp? Rpmin, and Rpmax?
Thanks,
Craig Beiferman
I only want LHR mode, and I measured the coil with no parallel capacitor. (Is this correct?)
Hi Craig,
If you measured the coil without a parallel capacitor, then the resonant frequency will be the coil's self resonance frequency (SRF). If you are unfamiliar with this term, section 2.5 of LDC Sensor Design explains it in more detail. This frequency is fairly unstable, so we recommend keeping the sensor frequency below 75% of the SRF. This is the major limitation for selecting a capacitance value. You can use the inductive sensing calculator tool to quickly calculate acceptable capacitance values for a target sensor frequency.
In LHR mode, Rpmax is not used and Rpmin is used to determine the sensor drive current. The parallel capacitor will change the sensor's Rp value. An equation in section 1.2 of LDC Sensor Design shows this relationship. Once you have selected a capacitor, connect it in parallel with your coil and remeasure Rp at the sensor's resonant frequency using the network analyzer. Use the minimum Rp (which looks like it will be the extended position) and Table 36 in the LDC1101 datasheet to set Rpmin.
Best Regards,