Other Parts Discussed in Thread: AWR1642,
Hi
AWR1642 SDK 02_01_00_04 module documentation had introduce the "Near Field Correction" and the AWR1642 demo support nearFieldCfg CLI command, but I do not see any related information in SDK 03_01_00_02 module documentation and also do not see nearFieldCfg CLI command in AWR1843 demo. I have questions:
(1) Does AWR1843 and SDK 03_01_00_02 also need to concern the Near Field Correation? if it is, can I reference SDK_02_01_00_04 correction result to correct it by manual before TI provide the CLI command?
(2) How about the Ele angle? Also need to do the near field correction? Does TI has the correction data for Ele angle?