This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: ES3.0

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

I find that   mmwave_sdk_03_01_01_02 contains the firmware    xwr12xx_xwr14xx_radarss_rprc.bin .And the  MMWAVE RadarSS Release Notes   says it support xWR1443 ES3.0 .

but when I  download it into  IWR1443BOOST . it can not be successful. Can you give me some advise? thank you.

volume_downVerboseClearClose

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Initialization complete.

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Flashing process starting...

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Connecting to COM Port COM3...

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Reset connection to device

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Set break signal

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Reading device version info...

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: ** 1 files specified for flashing.

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Checking file C:/ti/mmwave_sdk_02_01_00_04/firmware/radarss/xwr12xx_xwr14xx_radarss_rprc.bin for correct header for IWR1443.

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Header of C:/ti/mmwave_sdk_02_01_00_04/firmware/radarss/xwr12xx_xwr14xx_radarss_rprc.bin file indicates it is not a valid file to flash to IWR1443: 0x43525052

[2019/4/22 下午6:05:13] [ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Disconnecting from device on COM port COM3...

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...

[2019/4/22 下午6:05:13] [INFO] Cortex_R4_0: Instance deinitialized!