This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: TDC7200 and MEAS_COMPLETE_FLAG

Other Parts Discussed in Thread: TDC7200

Good day Colleagues,

My customer is evaluating the TDC7200 and got issue with the MEAS_COMPLETE_FLAG.

Could you review it and say what can be wrong in here or what customer has to check?

Please, see detailed description below:

1. TDC7200 setup:

  • TDC7200: in mode #2, one stop signal, calibration by 10 periods of CLOCK
  • START – 250 pulses with a duration of 250 nsec with a period of  2.5 msec
  • STOP – 250 pulses of duration no less than 1.0 usec, delayed by 1.5 msec relative to START pulses
  • control parameter is – MEAS_COMPLETE_FLAG

 

2.Results:

  • repetition factor: – no less than 100 times
  • issue is –  MEAS_COMPLETE_FLAG doesn't setup (while MEAS_STARTED_FLAG is set upped)
  • issue occurs from 1 to 4 times in each 250 pulses
  • issue doesn't not occur if period is increased up from 1.5 msec to  4 msec

Thank you, Mikhail