This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: CAN Bus instruction needed

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1642BOOST

We are working on AWR1843BOOST application. Now, we followed the guide for switch settings and have completed connection of power and CAN-H/CAN-L, but we could read nothing and there are limited information about CAN in user guide, especially CAN message definitions(CAN ID, values, etc.). Besides, we want to use MATLAB/Simulink as processing tool for the radar. Are there any instructions how to make it works?

  • Hi,

    We are not clear what application you are running on the AWR1843BOOST.

    In order to test the CAN output there are several options

    1) Use unit test provided in

    C:\ti\mmwave_sdk_03_01_00_02\packages\ti\drivers\canfd\test\xwr18xx

    2) Run the following lab binaries and check the CAN lines with a scope. Even if these binaries are built for AWR1642BOOST, they should also work for AWR1843BOOST

    mmwave_automotive_toolbox\labs\lab0005_object_data_over_can\odoc-target\pre-built-Binaries\AWR1642BOOST

    Thank you
    Cesar