Other Parts Discussed in Thread: AWR1642
Tool/software: Code Composer Studio
Question 1:
The documents show that the DDR data rate is twice the value of the Clock (e.g., 150 Mbps (75-mhz DDR Clock)). Is the data rate of SDR equal to the Clock rate?
Question 2:
Capture demo code has a DDR clock mux. What does this mean? Should it be in line with the DDR clock Settings?
Question 3:
In the capture demo, are the ADC buffer headers in the continuous mode of the LVDS data stream present on every transmission, or are they only present on the first transmission?
Question 4:
If you run capture demo's LVDS continuous flow mode, is board fever normal?
Question 5:
How can I change the LVDS clock rate in capture demo to a value that is not optional in demo?