This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: How could I change the IP address of DCA1000EVM and the destination IP ?

Part Number: DCA1000EVM


HI

I am going to connect multiple DCA1000EVM to PC

However, as their own IP is set to 192.168.33.180 and their destination IP is 192.168.33.30, I could not connect multiple DCA1000EVM to one PC

Also since my PC is set to certain IP address for other sensors, I have to also change destination IP address at DCA1000EVM.

I tried to change IP address of dca1000EVM by using lua scripts such as

ar1.CaptureCardConfig_EthInit_WithoutSPI

However it does not work when I send command to board.

How could I set a certain IP address for DCA1000EVM?

Do I need to do it on FPGA? If is does, what do I need to do it?

Thanks a lot

Jinhyeong Kim