Other Parts Discussed in Thread: ENERGIA
Hi:
Customer is now considering to add the function of Ultrasonic Distance Sensor on their products, they are currently evaluating the solution of PGA460, they lists some questions below and need our comments:
spec: Ultrasonic Motion detection at 15’-20’(3.8m~5.0m) range, with >140-degree FOV
Questions :
1, as for the driver type(direct driver and transformer driver), can you elaborate the difference between their power design circuit respectively? did these two types have some variation regarding the ability of product detection(distance and FOV)?
2: did TI have the success case of supporting the Uart interface control? so how about the firmware's porting, is it complicate?
3: so what kind of support related can TI support as for the firmware and hardware ?
4, as for this design spec, which solution is the best if considering the design difficulty and design / test schedule ?