Part Number: TDC1000-TDC7200EVM
Dear Sir,
I want to measure fuel level in diesel generator tank.
The tank dimensions are as follows:
1) 1200 * 900*900 mm^3
2) 1828*1706*252 mm^3
I have decided to use the part number SMD50T21F1000R(https://www.steminc.com/PZT/en/piezo-electric-disc-50x21mm-r-1-mhz) as the transducer interfaced with TDC1000-TDC7200EVM evaluation module.
Kindly help me with the following :
1) the parameters to enter on the TDC1000 for this diameter\thickness\power.
2) the installation position of the transducer is on the top inside of the generator tank.
Thanking You,
Nikita Pal