This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Which is better for people counting: IWR1642Boost or IWR6843ISK?

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR6843ISK, , IWR6843

Hi,

I have the IWR6843ISK and it works well for the people counting lab. 

How does the IWR1642Boost compare to it? Is one better for close range and the other better for long range?
I understand that both operate at different frequency ranges (60GHz vs 77 GHz).

Linus

  • Hi Linus,

    Moving forwards, we will only be updating the people counting lab for the IWR6843. These updates will improve quality of life, performance, and tunability of the demo. The frequency ranges are similar enough that we do not see a performance difference between the two devices.

    My recommendation is to use the IWR6843. (77 GHz will be limited to automotive space by regulation in most of the world as well)

    Regards,
    Justin