This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Transmit a continuous CW

Part Number: AWR1642BOOST


I have made a mmwave radar product, which uses the CAN interface and cannot be connected with DCA1000EVM.

Now I need to test the antenna in the single-frequency mode.How can I modify mmw demo to enable continuous mode function to test my radar product?

Looking forward to reply.Thank you!

  • Hi,
    mmw demo doesn't support continuous mode but you can refer capture demo application from old version of SDK (1.0) where that application supports to configure continuous mode and stream over LVDS.
    As you have mentioned that your board has CAN interface over which I hope you want to stream the raw data then refer this application where it sends object data over CAN-
    dev.ti.com/.../node


    Regards,
    Jitendra