This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: Need for more BPF center frequencies

Part Number: PGA970

Hi,

Starting from the PGA970 datasheet I could get the filter coefficients for BPF for center frequencies which are multiples of 1000 Hz (1000, 2000, 3000, ...) up to 20kHz, nevertheless in my application I also need half multiples of 1000 Hz (1500, 2500, 3500, ...). Can you provide me a table of coefficients for those frequencies, considering a bandwidth of 20, 100 and 250 Hz for them?

Thank you in advance.

Best regards,

Alessandro Cominelli