This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: 80GHz Capable Regulatory Test Labs

Part Number: AWR1642

Hello:  The 76-81GHz frequency range is not one supported by the many regulatory and certification test labs.  The frequency is simply above the 40GHz to 50GHz upper limit of most labs.  Can TI point to some labs that can perform regulatory testing on short range radars using chips such as the AWR1642?