This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: 3 Wire

Part Number: PGA970

Dear Scott,

 I managed to get the PGA970 finally  working. However, I am confused what is the biasing configuration required for a 3 wire (Half Bridge) setting. I have disabled  the S1 and S2   VCM_EN bit. and set SEM bit to 1. But I am facing a drift issue with readings shifting with time and not stable/fixed even with temperature compensation enabled. Also what should be the BPF and LPF filter cutoff settings in case I need to use a TESA probe as LVDT to measure a travel distance range of 4mm  with 0.1um resolution. Kindly take this as urgent and reply as soon as possible.  Thanks Anuj