This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: People Counting and Traffic Monitoring simultaneously

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi,

         I would like to use the IWR1642 for people counting and traffic monitoring simultaneously. We were able to run both separately by flashing the individual bins to the sensor to count people or monitor traffic. We were able to view both data displayed individually on the main_pplecount_viz_m(People counting GU)  and also on tm_demi.m(Traffic monitoring GUI). However, now we would like to flash both bins into the mmwave sensor so that the IWR1642 can run both  at the same time, and then take the data obtained from both, and plot it in a separate MATLAB GUI we created. Please how would you recommend we achieve that?

Thanks 

Ololade

  • Former Member
    0 Former Member
    Hello,

    You can only flash one image to the device. If you would like to modify the device behavior the source code is provided for both labs; please integrate the software as needed for your application. The proof of concept demos are provided as is additional features or different behavior will require user implementation.

    Amanda